Technical FAQs

Ask a Question

What breaker can be used in the old obsolete CU12L400B combination service entrance device that used the Q2L2200H Service Disconnects?

Issue:
Product design Features

Product Line:
Combination Service Entrance Devices

Environment:
Service Disconnects

Cause:
Application and or Maintenance

Resolution:
The Q2L2200H Service Disconnect is Obsolete and NO longer available, BUT has been replaced by the breaker catalog number QDL22200.

CTA-ID : 2016975
Was this helpful?
What can we do to improve the information ?