Technical FAQs

Ask a Question

Can the two normally open contacts on a RE7 timer with 2 output contacts be changed to instantaneous?

No. These are SPDT output contacts. The NO and NC contacts are not independent. A switch on the front face of the timer allows one SPDTcontact to be used in the instantaneous mode. The second SPDT contact is always timed.

CTA-ID : 2016966
Was this helpful?
What can we do to improve the information ?