Technical FAQs

Ask a Question

What is a 9080V3?

Issue:
What is a 9080V3?

Product Line:
Terminal Blocks

Environment:
All products

Cause:
Product Features

Resolution:

The 9080V1, V2 & V3 are a hard phenolic panel mount terminal block with solderless box lugs. The conductor range is #6 to 250 kcmil. The 9080V1 has 1 circuit, V2 has 2 and V3 has 3 circuits.



CTA-ID : 2016788
Was this helpful?
What can we do to improve the information ?