Technical FAQs

Ask a Question

What is the cutout size in a NQODQB for the QBL breaker handle and escutcheon ?

It is 1 3/4 `` wide x 3 1/2`` high. The NQODQB kit was designed for use on either top feed or bottom feed panels. The opening in the main breaker deadfront is larger than the actual breaker handle.


Revised 3/29/04


CTA-ID : 2016785
Was this helpful?
What can we do to improve the information ?