Technical FAQs

Ask a Question

What is the AIC rating for 9080GCB circuit protectors?

There is no AIC rating because the device is intended for supplementary protection per UL 1077 and not for use as a circuit breaker.

CTA-ID : 2017233
Was this helpful?
What can we do to improve the information ?