Technical FAQs

Ask a Question

Will the soft starter begin to ramp up from the present voltage or will it decel to a stop first if a start command is given during a deceleration ramp down on the LH4N2 ****?

The soft starter does not go to 0 VAC output when a start command is given during deceleration. The voltage will ramp up from the present output level.


CTA-ID : 2017111
Was this helpful?
What can we do to improve the information ?