Technical FAQs

Ask a Question

What is the contact rating of ZB6 contact blocks?

AC-15 they are rated NEMA B300,
DC-13 they are rated NEMA R300,
with a continuous thermal current rating of 5A.




CTA-ID : 2017075
Was this helpful?
What can we do to improve the information ?