Technical FAQs

Ask a Question

When the Altivar 66 drive is running by means of serial communication, can the custom fault feature be used?

The customer defined fault input does not operate when in serial link control. The drive must be in terminal command to respond to custom fault commands.


CTA-ID : 2016962
Was this helpful?
What can we do to improve the information ?