Technical FAQs

Ask a Question

What is the deadfront part number for an NQOD12M100CU or NQOD412M100CU interior?

Issue: 
Need replacement deadfront

Product Line:
NQOD Panelboards

Environment:
LV Panelboards

Cause: 
Replacement Parts

Resolution:
Each panel will require the following:

SINGLE PHASE INTERIOR
(1) NQODRPL12BFMB1 (obsolete)

THREE PHASE INTERIOR
(1) NQODRPL412BFMB1 (obsolete)

Both of these parts are now obsolete with no replacement.
Was this helpful?
What can we do to improve the information ?