Technical FAQs

Ask a Question

If the ATV58 Type N drive is ordered without the keypad display is the VW3A58836 closing plate included to cover the keypad opening?

Yes.
The closing plate part number VW3A58837 is included and already installed when this type drive is ordered without the keypad.


CTA-ID : 2016780
Was this helpful?
What can we do to improve the information ?