Technical FAQs

Ask a Question

What is the 1380 in catalog number KAL36200-1380?

1380 is a combination of two accessories -1021 and -1212. The 1021 is a shunt trip of 120, 208 or 240 volts ac and the 1212 is 1A/1B auxiliary switch.


CTA-ID : 2016774
Was this helpful?
What can we do to improve the information ?