Technical FAQs

Ask a Question

What terminations are available on the HCPSU8SN neutral assembly used in single row I-Line interiors?

Main Lugs: (8) #3/0 - 750MCM AL/CU

(2) Bar A: (34) #4 - 14 AWG AL/CU (Each Bar A = 17 terminations.)
(1) Bar C: (9) #14 - 1/0 AWG AL/CU
(1) Bar D: (7) #6 - 350MCM AL/CU

Revised 3/23/04



CTA-ID : 2016752
Was this helpful?
What can we do to improve the information ?