Technical FAQs

Ask a Question

What is the lug capacity on the ATV58HC23N4, ATV58HC25N4, ATV58HC28N4, ATV58HC31N4 or ATV58HC33N4?

These units ship without lugs.  Customer must supply lugs to fit selected wire size. The bus bars have 12 mm diameter hole designed to fit an M12 bolt. The hole is not threaded.

Actual wire size used shall be based on local codes and OCPD ratings.

Check for proper electrical clearances. For applications up to 600 V,
maintain at least 0.375 in. (9.53 mm) clearance between adjacent power terminal lugs and at least 0.5 in. (12.7 mm) clearance between
any live part and the device enclosure.


CTA-ID : 2017008
Was this helpful?
What can we do to improve the information ?