Technical FAQs

Ask a Question

How is an MHC--SHR or MHC--FHR trim attached to the box?

Captive hardware is used to attach the trim to the box lip and standard trim screws are used to secure it to the panel deadfront.

Revised 4/13/04

CTA-ID : 2017198
Was this helpful?
What can we do to improve the information ?