Technical FAQs

Ask a Question

Is a ground bar for an SU3040D400CB?

No ground bar is required. The Combination service entrance devices are for use as service entrance equipment only and the neutral is bonded to the enclosure at the factory. Use the neutral for the ground connections.

CTA-ID : 2017066
Was this helpful?
What can we do to improve the information ?