Technical FAQs

Ask a Question

How is the built in manual speed pot ordered on the ATV31 drive?

Add an `A` at the end of the part number. This option also includes Run and Stop / Reset push buttons on the face of the drive. This option is not available on the 575V units.

CTA-ID : 2017365
Was this helpful?
What can we do to improve the information ?