Technical FAQs

Ask a Question

What is the part number for the instruction sheet for the VW3A28101 remote mount keypad kit for the ATV28?

There is no published instruction sheet for this product on the SquareD website. There is a sheet that comes with the product that shows mounting instructions. The keypad mounting is similar to the VW3A58103 Altivar 58 remote keypad kit.

The bulletin number for the ATV58 remote mount kit is 8806DB0003. It can be downloaded from http://www.SquareD.com or http://ecatalog.squared.com/techlib/

The link below goes to a scanned copy of the actual instruction sheet for the VW3A31101 kit.


CTA-ID : 2016923
Was this helpful?
What can we do to improve the information ?