Technical FAQs

Ask a Question

Does the KC34250 breaker have an adjustable magnetic trip setting?

Yes, it has a dial type adjustable trip setting that is nominally 1250 amps on the low side and 2500 amps on the high side. It can be adjusted by means of a flat head screw driver.

CTA-ID : 2017059
Was this helpful?
What can we do to improve the information ?