Technical FAQs

Ask a Question

Why do we ship Homeline load centers with twist outs removed in position number 1 & 2 of the dead front trims?

The first twist out is the hardest to remove. The twist out are removed in order to make it easier to get the installation started.

CTA-ID : 2017057
Was this helpful?
What can we do to improve the information ?