Technical FAQs

Ask a Question

What does MAG-GARD refer to?

MAG-GARD (trademark) is the Square D family of instantaneous-trip or Magnetic only circuit breakers (also referred to as motor circuit protectors). These are used along with overloads to protect motor circuits.


CTA-ID : 2016937
Was this helpful?
What can we do to improve the information ?