Technical FAQs

Ask a Question

Does the D225NR come with a hub opening in the top and if not will it maintain the rating if one is cut in in the field?

It comes with a blank endwall and it can have a field cut opening but to keep it`s rating of N3R you need to use the H type hubs.



CTA-ID : 2017176
Was this helpful?
What can we do to improve the information ?