Technical FAQs

Ask a Question

Can an SDSA3650 be mounted in the gutter space of an NQOD panelboard?<br /><br /><br /><br />

The SDSA3650 can be installed in panelboards as a factory assembled option ONLY.


Revised 4/7/04




CTA-ID : 2017172
Was this helpful?
What can we do to improve the information ?