Technical FAQs

Ask a Question

Does the ATV28 Type H unit meet CE with the filter that is already installed in it or is and additional EMC filter required to get this rating?

The type H unit is CE marked and with the filter already installed in unit the drive meets CE mark for Class A (industrial) installations and for use in Class B (Residential) installations you do need to install the additional filter.


CTA-ID : 2029
Was this helpful?
What can we do to improve the information ?