Technical FAQs

Ask a Question

Are Homeline main breaker lugs rated for aluminum or copper conductors?

Yes the QOM1 & QOM2 main breaker will accept copper or aluminum conductors.


CTA-ID : 2016929
Was this helpful?
What can we do to improve the information ?