Technical FAQs

Ask a Question

What are the dimensions for the ATV31 H055N4?

Width 105 (4.13) Height 143 (5.63) Depth 150 (5.91)

Weight 1.35kg (2.92) lb

This is the same dimensions for HU11M2, HU15M2, HU22M3X, H037N4, H055N4, H075N4, HU11N4, HU15N4, H075S6X and HU15S6X units.


CTA-ID : 2017355
Was this helpful?
What can we do to improve the information ?