Technical FAQs

Ask a Question

What are the dimensions and weight for ATV28HU09M2U, ATV28HU18M2U, Altivar 28 drive?

Width = 4.134 in (105 mm) , Height = 5.118 in (130 mm), Depth = 5.512 in (140 mm)
The weight is 4.0 lbs (1.8 kg)

This information can be obtained in the ALTIVAR 28 Adjustable Speed Drive Controllers User`s Guide, Document Number: VVDED399062US



CTA-ID : 2016152
Was this helpful?
What can we do to improve the information ?