Technical FAQs

Ask a Question

What is maximum number of outlets that can be protected on a GFI breaker circuit?

Square D does not limit the number of outlets that can be connected to one circuit. Check with local codes.


CTA-ID : 2016145
Was this helpful?
What can we do to improve the information ?