Technical FAQs

Ask a Question

Can the head be moved 90 degrees on a 9007C54F?

Yes the operating head can be moved IN 90 degree increments through 360 degrees.


CTA-ID : 2016143
Was this helpful?
What can we do to improve the information ?