Technical FAQs

Ask a Question

What is the XB4 contact block DC voltage rating when applied as part of the XD4PA joystick?

DC supply:
Utilization category DC-13
Standard single or double blocks with screw clamp terminals:
R300: Ue=125VDC and Ie=0.22A or Ue=250VDC and Ie=0.1A

CTA-ID : 2016696
Was this helpful?
What can we do to improve the information ?