Technical FAQs

Ask a Question

How do the preset speeds operate when using 2 presets with the Altivar 58 drive?

See attached keypad programming manual for additional details.

For 2 preset speeds, one logic input is used. One logic input must be programmed for PS2 (2 preset speeds). There should not be any other preset speeds programmed to other logic inputs. If the input is high and the drive is running the drive will run at HSP (high speed). If the input is low, the drive will run at LSP + AI reference (Low speed plus whatever analog speed reference may be applied). High speed (HSP) and Low speed (LSP) can be set in the SET adjustment menu 2.


CTA-ID : 2015915
Was this helpful?
What can we do to improve the information ?