Technical FAQs

Ask a Question

What is the difference between a 9001KYSS2 and a 9001KYSS200?

Issue:
What is the difference between a 9001KYSS2 and a 9001KYSS200?

Product Line:
Control Stations

Environment:
All products

Cause:
Product Features

Resolution:
The 9001 KYSS2 is a 2 hole stainless steel control station enclosure. The 9001 KYSS200 indicates a custom assembled pushbutton station built with the KYSS2 enclosure. The 9001KYSS200 requires a key sheet be filled out.


CTA-ID : 13484
Was this helpful?
What can we do to improve the information ?