Technical FAQs

Ask a Question

What is the heat dissipation for the 150 HP, 460 VAC, VT, ATV58HC13N4XZU drive at rated load?

The Dissipated power for this drive is 2750 Watts at rated load.

See the Instruction Bulletin VVDED397048US ALTIVAR 58 TRX Adjustable Speed Drive Controllers Installation Guide for Type H Controllers for additional mounting and cooling guidelines.

CTA-ID : 2016293
Was this helpful?
What can we do to improve the information ?