Technical FAQs

Ask a Question

Are lugs available for the compact CM breaker?

No, Compact CM breakers are bus-connected only. For cable connection, lugs can be applied to customer-supplied bus using customer supplied mechanical lugs or compression connectors.
Rear connectors are included when required (2000-2500A UL; 3200A IEC), and are available for purchase as replacements or for rear connection of lower-amperage breakers if desired.

CTA-ID : 445
Was this helpful?
What can we do to improve the information ?