Technical FAQs

Ask a Question

Is there an Ethernet card available for the Altivar 28 drive?

No.
The ATV28 communicates by Modbus protocol out of the RJ45 port on the front of the unit.
To communicate using Ethernet would require a bridge or gateway. There is no Square D recommended part for this application.


CTA-ID : 2016686
Was this helpful?
What can we do to improve the information ?