Technical FAQs

Ask a Question

Does Square D offer a 225 Amp rated, three phase, sub feed lug kit for use in the three phase QO load centers?

Issue:
Product Features

Product Line:
QO Three Phase Load Centers

Environment:
Accessories

Cause:
Application

Resolution:
NO, Square D does not offer a 225amp rated sub-feed lug kit for the 3-phase QO load centers. The maximum sub-feed lug kit Square D offers is 125amp, catalog number QO3125SL. 


CTA-ID : 2016506
Was this helpful?
What can we do to improve the information ?