Technical FAQs

Ask a Question

What are the dimensions and weight of the ATV58HC13N4XZU, ATV58HC15N4XZU or ATV58HC19N4XZU drive?

The dimensions are 18.9 inches (480 mm) wide, 27.2 inches (690 mm) High, and  15.7 inches (400 mm) deep .

The weight is 169 lb (77 kg).

CTA-ID : 2016292
Was this helpful?
What can we do to improve the information ?