Technical FAQs

Ask a Question

What are the rail and deadfront extensions required to mount an NQOD442L600 in an MH62?

The following parts will be required per panel and can only be installed at the mains end:

(1) 80120-823-02 6`` left rail extension
(1) 80120-824-02 6`` right rail extension
(1) 80110-876-02 MLO cover 6`` extension
(4) 21590-17081 Rail extension screws


Revised 3/2/04




CTA-ID : 2014793
Was this helpful?
What can we do to improve the information ?