Technical FAQs

Ask a Question

Do the GS1 switches have horsepower ratings?

Yes. They are as follows:

Switch Voltage Max. HP Rating/Max. Motor FLC
GS1 30A 240V 7.5/22
480V 15/21
600V 20/22
125Vdc 3/25
250Vdc 5/20
GS1 60A 240V 15/42
480V 30/40
600V 50/52
125Vdc 3/25
GS1 100A 240V 30/80
480V 60/77
600V 75/77
125Vdc 7.5/58
250Vdc 20/38
GS1 200A 240V 60/154
480V 125/156
600V 150/144
125Vdc 15/112
250Vdc 40/140 (w/3poles in series in one of the following conditions: 3 poles on +, 2 poles on + and 1 on -, 1 pole on + and 2 on -, 3 poles on -).
GS1 400A 240V 125/312
480V 250/302
600V 350/336
125Vdc 20/148
250Vdc 50/173 (w/3poles in series in one of the following conditions: 3 poles on +, 2 poles on + and 1 on -, 1 pole on + and 2 on -, 3 poles on -).
GS1 600A 240V 250/602
480V 500/590
600V 500/472
GS1 800A 240V 250/602
480V 500/590
600V 500/472


CTA-ID : 2016288
Was this helpful?
What can we do to improve the information ?