Technical FAQs

Ask a Question

Does the U-Line control module need a voltage code?

Yes. With U-Line products, the voltage code is incorporated in the control unit instead of the starter base.


CTA-ID : 2016234
Was this helpful?
What can we do to improve the information ?