Technical FAQs

Ask a Question

Can a EZM1400CBU, 400 amp main breaker device, be modified to a EZM1600CBU, 600 amp main breaker?

Issue:
Product Design Features

Product Line:
EZM Metering

Environment:

Cause:
Application

Resolution:
No, the 400amp EZM1400CBU main breaker device, cannot be modified to a 600 amp main breaker device. Would need to obtain the 600amp device.


CTA-ID : 2016113
Was this helpful?
What can we do to improve the information ?