Technical FAQs

Ask a Question

Why can`t I select single pole breakers for a NQOD 240 volt panel in the product selector?

240 volts is a 3 phase 3 wire system which does not have a neutral. A single pole breaker requires a neutral to complete the circuit. Without a neutral, there is no way to use a single pole breaker, which is why it is locked out in the product selector.


Revised 3/10/04



CTA-ID : 2015832
Was this helpful?
What can we do to improve the information ?