Technical FAQs

Ask a Question

What is the difference between spaces & 1-pole circuits in a QO loadcenter?

Issue:
Product Features

Product Line:
QO LC

Cause:
Clarifying product features differences

Resolution:
Spaces are just that, spaces. You can use a 2 pole circuit breaker for a 240V circuit that takes up 2 spaces in the load center, and you can get a QOT tandem breaker that has two 1 pole circuits that takes up only 1 space.


CTA-ID : 2016280
Was this helpful?
What can we do to improve the information ?