Technical FAQs

Ask a Question

Can padlock attachment, cat. no. 26970, for IEC 947-2 rated Multi 9 C60 miniature circuit breakers be used for 1, 2, and 3 pole devices?

Yes, the 26970 can be used for 1, 2, and 3 pole devices.


CTA-ID : 2016278
Was this helpful?
What can we do to improve the information ?