Technical FAQs

Ask a Question

Does the 9012 Type G pressure switch come standard with a Pilot Light?

NO, this is a factory modification, for factory modifications see Digest 173 page 20-8.

For replacements or field installation see Digest 173 page 20-10.

CTA-ID : 2016432
Was this helpful?
What can we do to improve the information ?