Technical FAQs

Ask a Question

What are the part numbers for a 12`` x 6`` to 8`` x 8`` and a 8`` x 8`` to 4`` x 4`` NEMA 12 reducer?

A reducer is not available to go directly from 12`` x 6`` to 8`` x 8``. The LJB86R and LJB64R are used together to step down from 8`` x 8`` to 4`` x 4``.


CTA-ID : 2016633
Was this helpful?
What can we do to improve the information ?