Technical FAQs

Ask a Question

Is the 9070 Type SK transformer Disconnect offered without the Transformer (essentially a switch and enclosure with options)?

Issue:
Transformer Disconnect modifications

Product Line:
LV Transformers

Environment:
Applies to 9070 SK Transformer Disconnects by SquareD/Schneider Electric

Cause:
9070 Transformer Disconnects have possible modifications

Resolution:

SquareD/Schneider Electric does not offer the 9070 Type SK product without a Transformer.


CTA-ID : 2016627
Was this helpful?
What can we do to improve the information ?