Technical FAQs

Ask a Question

Why is there is a warning label on a PTQ3680GH that states this device cannot be used on 800A copper I-line II busway?

The 800A copper busway has a narrow bus bar which will not allow that unit to properly plug in. It can be used on aluminum busway and larger copper amperage busways because they have larger bus bars.


CTA-ID : 2016484
Was this helpful?
What can we do to improve the information ?