Technical FAQs

Ask a Question

What is the IP or NEMA enclosure rating for the open ATV58 Type H drive?

ATV58HU09M2 to ATV58HU90N4: IP20/open type controllers according to Standard EN50178.
ATV58HU90M2 to D46M2, ATV58HD12 to D79: UL Type 1 with conduit connection kit.
ATV58HC10N4X to C33N4X: IP20 all surfaces except the bottom. IP00 on the bottom due to the power connections

CTA-ID : 2015879
Was this helpful?
What can we do to improve the information ?