Technical FAQs

Ask a Question

Is an 8606 autotransformer starter available as a combination starter with a non fusible disconnect ?

Yes, through NEMA size 5. Use Form Y792 to add a non fusible disconnect.


CTA-ID : 2016442
Was this helpful?
What can we do to improve the information ?