Technical FAQs

Ask a Question

What rating of potentiometer can be used on Altivar 28 drive?

1k ohms to 10k ohms.
The power supply is 10 VDC with 10 mA maximum current. It is protected from short circuits and overload.
Could use ATVPOT25K. It is a 22 mm operator with a pot that is 2,500 ohms.


CTA-ID : 2016473
Was this helpful?
What can we do to improve the information ?